FRWY-LS1012A develop environment setup

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FRWY-LS1012A develop environment setup

1,896 Views
zcchai
Contributor I

Hi NXP team and community,

I have a FRWY-LS1012A board and want to set up my development environment for it. I noticed the board was used to be developed under CodeWarrior, however, that was for QorIQ old SDK(say Yocto based), right? So the questions are:

1) If I want to use Layerscape SDK(LSDK), what kind of IDE do you recommend? 

2) What JTAG device do you recommend? so I can download bootloader for the bricked board and debug.

3) Any good practice how to build and debug? e.g, Build on host and download to the board ? or directly build on target?

Thanks

0 Kudos
Reply
2 Replies

1,655 Views
Pavel
NXP Employee
NXP Employee

1) Use Ubuntu 18.04 for LSDK 18.09.

 

Use the following command sequence for LSDK 18.09 installing:

$ sudo apt-get install git

$ tar xvzf flexbuild_lsdk1809.tgz

$ cd flexbuild

$ source setup.env

 

wget http://www.nxp.com/lgfiles/sdk/lsdk1809/app_components_arm64.tgz

flex-builder -i mkrfs -a arm64

 

wget http://www.nxp.com/lgfiles/sdk/lsdk1809/arm64-modules-4.14.67.tgz

tar xvzf app_components_arm64.tgz -C build/apps

sudo tar xvzf arm64-modules-4.14.67.tgz -C build/rfs/rootfs_ubuntu_bionic_arm64/lib/modules

 

flex-builder -i merge-component -a arm64

 

flex-builder -i compressrfs -a arm64

 

2) Use CodeWarrior TAP and CodeWarrior Development Suite for Networked Applications:

 https://www.nxp.com/support/developer-resources/software-development-tools/codewarrior-development-t...

 

3) Usually your host is used for application compiling. For example NFS file system can be used for using testing this application on your board.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,655 Views
zcchai
Contributor I

Hi Pavel,

Thanks for the information. I have some follow up questions:

1. Regarding to the Jtag, can I just use CMSIS-DAP through USB, instead of CodeWarrior TAP?

2. I remember there used to be special/free version of CodeWarrior, is this still true for the latest CW?

3. I want to test with OP-TEE setup, is there any procedure to do that?

Thanks

Zhenchuan

0 Kudos
Reply