ETHERNET CONTROLLER OF LS1046A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ETHERNET CONTROLLER OF LS1046A

2,364 Views
Ellu24
Contributor III

Hi

I am designing a hardware using LS1046 and I want to connect ethernet PHY VSC8502-03 , which uses RGMII MAC interface, so that I have to connect that to EC module of processor. My questions are: 

1) what should I connect to EC1_GTX_CLK125 pin( any external crystal or clock generator Si 5332 output or any pins from ethernet PHY)

2)If I am not using EC2 , Can I left it unconnected?

3) Should I use synchronous ethernet as specified in VSC8502-03 datasheet, where should I connect RCVRDCLK1,RCVRDCLK2, CLK_SQUELCH_IN. (I have attached VSC8502-03 datasheet. Please find the attachment) 

Thanks in advance

0 Kudos
Reply
1 Reply

2,331 Views
yipingwang
NXP TechSupport
NXP TechSupport
0 Kudos
Reply