Does LS1024A's DDR3 controller support write leveling?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does LS1024A's DDR3 controller support write leveling?

1,596 Views
chenechun
Contributor I

       Does LS1024A's DDR3 controller support write leveling?When routing the address and command traces,can we use fly-by topology?We find that T-type topology is used in the LS1024ARDB.

        Another question, where can we download the LS1024ARM(reference manual) ?

Labels (1)
0 Kudos
Reply
2 Replies

1,512 Views
Bulat
NXP Employee
NXP Employee

Yes, write leveling is supported.

LS1024A is a regular NXP processor as many others, there is no document called LS1024ARM (reference manual). All available documentation can be found on the product page:

QorIQ® Layerscape 1024A | NXP 

Regards,

Bulat

0 Kudos
Reply

1,512 Views
chenechun
Contributor I

Thank you for your reply.As we know, there is a document called reference manual for many other NXP processor models.We can find information such as memory map, register description in the reference manual. But LS1024A only provides us a document called data sheet which doesn't have more detailed information.

0 Kudos
Reply