Debug Option

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Debug Option

1,586 次查看
g_reshmi
Contributor II

Hi NXP Team,

We are planning to develop a custom board based on LS1012A but we have space constraint. So we are planning to go with JTAG instead of CMSIS DAP for programming and debugging. Would that be fine?. 

Also kindly mention the additional changes that would be required if go with the above mentioned design.

Also will be compromising on any functionality if we avoid CMSIS DAP?

Can you please explain the use case of CMSIS_DAP(MK20DX128VFM5) Interface?

This CMSIS-DAP is used in all reference designs of LS1012A, so please clear this doubt and share interface diagram

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

1,578 次查看
ufedor
NXP Employee
NXP Employee

CMSIS-DAP is a low-speed debugger, accessible from the USB.

 

> we are planning to go with JTAG instead of CMSIS DAP for programming

> and debugging. Would that be fine?

Yes, it will be.

CMSIS-DAP is an optional module - i.e. JTAG can be used for the board bring-up solely.

 

> Also kindly mention the additional changes that would be required if go with the above mentioned design.

Just not implement the CMSIS-DAP module.

 

> Also will be compromising on any functionality if we avoid CMSIS DAP?

The whole LS1012A debug functionality is available through JTAG interface.

 

> Can you please explain the use case of CMSIS_DAP(MK20DX128VFM5) Interface?

Please refer for example to the QorIQ LS1012A Reference Design Board Manual, 2.18.1 CMSIS-DAP.

0 项奖励
回复