DDR PHY: 1D training failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR PHY: 1D training failed

4,884 Views
muaxi8
Contributor V

I have downloaded the Flash DDR Fip Binary to the address XSPI Nor 0x800000.

When I connected to the LX2080A (LX2160A Family) using CodeWarrior, I received the following error:

 DDR PHY: 1D training failed

muaxi8_0-1619851916224.png

What causes it and how can I fix it ?

My board‘’s uboot is now unable to get up, I guess that is the reason

Looking forward to reply

Tags (1)
0 Kudos
Reply
6 Replies

4,794 Views
eneyland
Contributor I

I am having this issue as well, would like to know the solution others had to clear it.

0 Kudos
Reply

4,874 Views
ufedor
NXP Employee
NXP Employee

Which board is in question?

How DDR SDRAM is implemented?

Which code is debugged?

What are the steps required to replicate the issue?

0 Kudos
Reply

4,859 Views
muaxi8
Contributor V

Has been resolved

thanks!!

0 Kudos
Reply

4,490 Views
deepanrajanbara
Contributor IV

Hi

Please let know , how the issue was resolved.

 

Thank you,

Deepanraj.A

0 Kudos
Reply

4,815 Views
xmj
Contributor I

I have met the similar issue.  Could you post the solution?

 

Thanks in advance! 

0 Kudos
Reply

4,851 Views
ufedor
NXP Employee
NXP Employee

Could you please explain the issue cause and the cure?

0 Kudos
Reply