DDR PHY: 1D training failed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DDR PHY: 1D training failed

4,924件の閲覧回数
muaxi8
Contributor V

I have downloaded the Flash DDR Fip Binary to the address XSPI Nor 0x800000.

When I connected to the LX2080A (LX2160A Family) using CodeWarrior, I received the following error:

 DDR PHY: 1D training failed

muaxi8_0-1619851916224.png

What causes it and how can I fix it ?

My board‘’s uboot is now unable to get up, I guess that is the reason

Looking forward to reply

タグ(1)
0 件の賞賛
返信
6 返答(返信)

4,834件の閲覧回数
eneyland
Contributor I

I am having this issue as well, would like to know the solution others had to clear it.

0 件の賞賛
返信

4,914件の閲覧回数
ufedor
NXP Employee
NXP Employee

Which board is in question?

How DDR SDRAM is implemented?

Which code is debugged?

What are the steps required to replicate the issue?

0 件の賞賛
返信

4,899件の閲覧回数
muaxi8
Contributor V

Has been resolved

thanks!!

0 件の賞賛
返信

4,530件の閲覧回数
deepanrajanbara
Contributor IV

Hi

Please let know , how the issue was resolved.

 

Thank you,

Deepanraj.A

0 件の賞賛
返信

4,855件の閲覧回数
xmj
Contributor I

I have met the similar issue.  Could you post the solution?

 

Thanks in advance! 

0 件の賞賛
返信

4,891件の閲覧回数
ufedor
NXP Employee
NXP Employee

Could you please explain the issue cause and the cure?

0 件の賞賛
返信