Console port accessing issue with LS1021ATSN-PA from Windows 10

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Console port accessing issue with LS1021ATSN-PA from Windows 10

3,182 Views
Abhilash_PV
Contributor I

Hi,

I'm working on a LS1021ATSN-PA development board. I'm facing an issue with its console port access from my Windows 10 PC. As mentioned in the quick start guide, I've connected the board's Micro USB console port to my PC using the Micro-B USB cable. The cable connection detected at the PC and appeared as a USB Mass Storage Device under the USB controllers of the Device Manager. But it does not appear as a COM port. I found a note from the MBED saying that Windows 10 does not require a specific serial driver to enable the COM port, however an older version of Windows 8 or lesser requires it. In my Windows 10 PC I cannot find the virtual COM port corresponding to this USB connection.

How do I resolve the issue? Kindly help me to proceed on it. 

Thank You.

Labels (1)
0 Kudos
Reply
8 Replies

2,203 Views
Youngsoo_do
Contributor III

Any solution to this problem?

0 Kudos
Reply

3,166 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the attached document to write CMSIS-DAP firmware image k22fx512_if_mbed.bin on  your target board.

0 Kudos
Reply

3,156 Views
Abhilash_PV
Contributor I

Thank you for the response.

I have followed the steps mentioned in the document to update CMSIS-DAP firmware on the board and it updated successfully. However I could not get the console port appeared as virtual COM port on my Windows10 PC. I have also tried the workaround suggested in one of the community question links (https://community.nxp.com/t5/Layerscape/LS1043ARDB-PD-USB-console-can-t-work/m-p/798002?commentID=10...) but it didn't help me either. On my PC I'm still getting it as USB Mass Storage Device only, and in the Teraterm application I cannot select the virtual COM port to connect with the board's console port. 

0 Kudos
Reply

3,138 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please make sure that you used CMSIS-DAP firmware image k22fx512_if_mbed.bin.

Please refer to the section "5. Windows mbed USB driver" in the document to install mbed USB driver.

There is a known issue with MBED operation under Windows 10:

        https://os.mbed.com/blog/entry/DAPLink-bootloader-update/

        This is the workaround we have confirmed to fix the mbed issue on Windows 10 PC's:

        - Go to the "Start" option on the PC and type the command  " services.msc"

        - Than you should see the following "Services" window open

        - Select the "Storage Services" and on the left-hand side of the window click the "Stop the service"

0 Kudos
Reply

3,101 Views
Abhilash_PV
Contributor I

I've followed the same steps mentioned along with the Windows 10 workaround procedure. But it did not solve my issue. 

After copying CMSIS-DAP firmware image "k22fx512_if_mbed.bin" into the "BOOTLOADER" named drive, the 'K22' marked status LED on the board blinks very fast. Then on unplugging and re-plugging of USB cable caused a drive named "MBED" appears on my PC. No virtual COM port is being created corresponding to the console port. I have re-enabled "Storage Services" in my PC and checked again. No difference observed (Only "MBED" drive appeared and no virtual COM port). 

MBED DriveMBED Drive

I have noticed a file named "fail.txt" in the "MBED" drive path as shown above. Content inside the text file is "SWD ERROR".

Am I right in the procedure that I followed? Is there any other image I've to use further to the above procedure?

0 Kudos
Reply

3,093 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please try the attached firmware image.

After plug in USB cable, please wait for while until the system is stable.

0 Kudos
Reply

3,089 Views
Abhilash_PV
Contributor I

I have tried this one but no difference in behavior observed. 

0 Kudos
Reply

2,842 Views
reginaldstjohn
Contributor III

We are seeing the same issue. Installed the k22fx512_if_mbed.bin, turned off the service "Storage Service" (There is no Storage Services),

Still no com port showing up in Windows 10 as of Oct-2021

0 Kudos
Reply