Codewarrior TAP USB can't connect

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Codewarrior TAP USB can't connect

2,503件の閲覧回数
zhoujianyun19
Contributor III

I use CodeWarrior TAP debug LS1043ARDB. But CodeWarrior TAP USB can't connect my compute.

My CodeWarrior  Development Studio configure as follows:

1.png

Errior log as follows:

2.png

3.png

ラベル(1)
タグ(1)
0 件の賞賛
返信
4 返答(返信)

2,297件の閲覧回数
ufedor
NXP Employee
NXP Employee

Which OS is installed on the computer?

Which CodeWarrior version is installed?

You wrote "CodeWarrior TAP USB" - which exactly TAP is used?

Have you tried to uninstall and reinstall the CodeWarrior?

0 件の賞賛
返信

2,297件の閲覧回数
zhoujianyun19
Contributor III

My system is windows 7.

CodeWarrior version is 11.2.0.

I tried to reinstall the CodeWarrior .

0 件の賞賛
返信

2,297件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please run "Diagnose Connection" and provide the log

DC.jpg

0 件の賞賛
返信

2,297件の閲覧回数
ufedor
NXP Employee
NXP Employee

Your version is not the latest.

Do you see v2017.03 in available CW downloads?

CodeWarrior ARMv8 64 bit|NXP 

0 件の賞賛
返信