Codewarrior TAP USB can't connect

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Codewarrior TAP USB can't connect

2,523 Views
zhoujianyun19
Contributor III

I use CodeWarrior TAP debug LS1043ARDB. But CodeWarrior TAP USB can't connect my compute.

My CodeWarrior  Development Studio configure as follows:

1.png

Errior log as follows:

2.png

3.png

Labels (1)
Tags (1)
0 Kudos
Reply
4 Replies

2,317 Views
ufedor
NXP Employee
NXP Employee

Which OS is installed on the computer?

Which CodeWarrior version is installed?

You wrote "CodeWarrior TAP USB" - which exactly TAP is used?

Have you tried to uninstall and reinstall the CodeWarrior?

0 Kudos
Reply

2,317 Views
zhoujianyun19
Contributor III

My system is windows 7.

CodeWarrior version is 11.2.0.

I tried to reinstall the CodeWarrior .

0 Kudos
Reply

2,317 Views
ufedor
NXP Employee
NXP Employee

Please run "Diagnose Connection" and provide the log

DC.jpg

0 Kudos
Reply

2,317 Views
ufedor
NXP Employee
NXP Employee

Your version is not the latest.

Do you see v2017.03 in available CW downloads?

CodeWarrior ARMv8 64 bit|NXP 

0 Kudos
Reply