Hi all,
Is there the posibility to adjust the internal connection of the RB signals?
This question comes up because we want to use the CS[6] of the IFC in GASIC mode which requires an and ready indication. For this ready indication RB[3] is used for 25-bit addressing. But even the RB[3] is multiplext with IFC_CS[5] ... to make now this RB[3] available over the RCW we lose the IFC_C[4] - IFC_CS[6] .... mhhhhh this is realy confusing!
So is there a way to set the internal connectivity of the RB signals like it is assigned for 28-bit addressing where nearly all RB signal are muxed on RB[0] exept RB[1]?
We realy appreciate your response.
Best regards and thank you in advance,
Christian