Can LS1046 update the program without uboot?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can LS1046 update the program without uboot?

1,204 Views
Hmc510
Contributor II

I noticed that LS1046 supports two startup modes:TF CARD/ QSPI FLASH.

Can LS1046 update the program without uboot? 

For example, The QSPI Flash is erased. Is there any other way to program firmware image without using the TF card boot mode.

 

Thanks

0 Kudos
Reply
2 Replies

1,171 Views
stadium_aquino
Contributor IV
0 Kudos
Reply

1,187 Views
Chavira
NXP TechSupport
NXP TechSupport

Thank you for contacting NXP support!

With the CodeWarrior TAP, you have to boot the board from RAM and then you can use the flash programmer tool in CodeWarrior.

Search | NXP Semiconductors

0 Kudos
Reply