Can LS1046 update the program without uboot?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can LS1046 update the program without uboot?

1,227件の閲覧回数
Hmc510
Contributor II

I noticed that LS1046 supports two startup modes:TF CARD/ QSPI FLASH.

Can LS1046 update the program without uboot? 

For example, The QSPI Flash is erased. Is there any other way to program firmware image without using the TF card boot mode.

 

Thanks

0 件の賞賛
返信
2 返答(返信)

1,194件の閲覧回数
stadium_aquino
Contributor IV
0 件の賞賛
返信

1,210件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

Thank you for contacting NXP support!

With the CodeWarrior TAP, you have to boot the board from RAM and then you can use the flash programmer tool in CodeWarrior.

Search | NXP Semiconductors

0 件の賞賛
返信