CLOCK BUFFER 9dmv0431akilf

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CLOCK BUFFER 9dmv0431akilf

Jump to solution
5,801 Views
Ellu24
Contributor III

I wish to use 9dmv0431akilf clock buffer as in reference design. what is DNP resistor mean and is it necessary to use? why VSW mode is connected to both power supply and gnd using dnp?

Thanks in advance

0 Kudos
Reply
1 Solution
5,777 Views
teddy_gom_e
Contributor III

This is not mandatory. this is just to ease schematics when you're unsure of option you want or when you want to have a pcb for multiple usage.

 

If you know exactly what you want, example  pin X to  VCC, set this resistor and do not add the other one to your schematic and you will not need to set an unused resistor to "DNP" state.

View solution in original post

3 Replies
5,788 Views
Ellu24
Contributor III

So is it necessary to add both when I design as shown in figure  and is DNP resistor same as that of normal resistor?

0 Kudos
Reply
5,778 Views
teddy_gom_e
Contributor III

This is not mandatory. this is just to ease schematics when you're unsure of option you want or when you want to have a pcb for multiple usage.

 

If you know exactly what you want, example  pin X to  VCC, set this resistor and do not add the other one to your schematic and you will not need to set an unused resistor to "DNP" state.

5,794 Views
teddy_gom_e
Contributor III

DNP : Do Not Populate.

 

This is cabling option when you want multiple options on a PCB.