CLOCK BUFFER 9dmv0431akilf

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CLOCK BUFFER 9dmv0431akilf

ソリューションへジャンプ
5,799件の閲覧回数
Ellu24
Contributor III

I wish to use 9dmv0431akilf clock buffer as in reference design. what is DNP resistor mean and is it necessary to use? why VSW mode is connected to both power supply and gnd using dnp?

Thanks in advance

0 件の賞賛
返信
1 解決策
5,775件の閲覧回数
teddy_gom_e
Contributor III

This is not mandatory. this is just to ease schematics when you're unsure of option you want or when you want to have a pcb for multiple usage.

 

If you know exactly what you want, example  pin X to  VCC, set this resistor and do not add the other one to your schematic and you will not need to set an unused resistor to "DNP" state.

元の投稿で解決策を見る

3 返答(返信)
5,786件の閲覧回数
Ellu24
Contributor III

So is it necessary to add both when I design as shown in figure  and is DNP resistor same as that of normal resistor?

0 件の賞賛
返信
5,776件の閲覧回数
teddy_gom_e
Contributor III

This is not mandatory. this is just to ease schematics when you're unsure of option you want or when you want to have a pcb for multiple usage.

 

If you know exactly what you want, example  pin X to  VCC, set this resistor and do not add the other one to your schematic and you will not need to set an unused resistor to "DNP" state.

5,792件の閲覧回数
teddy_gom_e
Contributor III

DNP : Do Not Populate.

 

This is cabling option when you want multiple options on a PCB.