CLOCK BUFFER 9dmv0431akilf

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

CLOCK BUFFER 9dmv0431akilf

跳至解决方案
5,800 次查看
Ellu24
Contributor III

I wish to use 9dmv0431akilf clock buffer as in reference design. what is DNP resistor mean and is it necessary to use? why VSW mode is connected to both power supply and gnd using dnp?

Thanks in advance

0 项奖励
回复
1 解答
5,776 次查看
teddy_gom_e
Contributor III

This is not mandatory. this is just to ease schematics when you're unsure of option you want or when you want to have a pcb for multiple usage.

 

If you know exactly what you want, example  pin X to  VCC, set this resistor and do not add the other one to your schematic and you will not need to set an unused resistor to "DNP" state.

在原帖中查看解决方案

3 回复数
5,787 次查看
Ellu24
Contributor III

So is it necessary to add both when I design as shown in figure  and is DNP resistor same as that of normal resistor?

0 项奖励
回复
5,777 次查看
teddy_gom_e
Contributor III

This is not mandatory. this is just to ease schematics when you're unsure of option you want or when you want to have a pcb for multiple usage.

 

If you know exactly what you want, example  pin X to  VCC, set this resistor and do not add the other one to your schematic and you will not need to set an unused resistor to "DNP" state.

5,793 次查看
teddy_gom_e
Contributor III

DNP : Do Not Populate.

 

This is cabling option when you want multiple options on a PCB.