Booting LS2085a with QSPI

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Booting LS2085a with QSPI

2,177件の閲覧回数
jitenpatel
Contributor II

Hi, I am working on LS2085a based custom board. The board is designed taking LS2085aqds as a reference but we don't have NOR as well as NAND flash in our board.We are using QSPI as our main booting device.

I want to know what are the memory mappings required for QSPI boot. Can we use code warrior for flashing images to QSPI flash or any separate tool is required. Nothing is mentioned in the Code-warrior Development Studio for QorIQLS series - ARM V8 ISA  Targeting Manual document that explains regarding flashing procedure for  QSPI.

ラベル(1)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

1,896件の閲覧回数
ufedor
NXP Employee
NXP Employee

CodeWarrior for ARM contains Flash Programmer module capable performing SPI Flash programming.

Please refer to the ARM V8 ISA, Targeting Manual, 7.7 Using flash programmer from eclipse IDE. In the section "7.7.2 Device selection and information" it is explained how Flash device is selected and SPI Flash devices also could be chosen.

0 件の賞賛
返信

1,896件の閲覧回数
jitenpatel
Contributor II

Hi

Thanks for your quick reply. we have already referred to the document mentioned by you but we are not getting QSPI flash in the device list. A snapshot is added below.WhatsApp-Image-20160509.jpg

can you please tell what are the other options available to flash images to QSPI.

0 件の賞賛
返信

1,896件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please check whether used SPI Flash is compatible with one explicitly supported by the Flash Programmer.

0 件の賞賛
返信