Autoboot won't stop

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Autoboot won't stop

3,662件の閲覧回数
matthuang
Contributor I

When I'm starting the LS1012ARDB board and the U-Boot message prompts me to hit any key to stop autoboot, I tried hitting keys but the terminal did not respond. I tried multiple cables so I don't think cable connection is the problem.

What might be causing this issue?

I looked at this thread but it didn't seem to help me:

https://community.nxp.com/thread/323089 

Thanks

ラベル(1)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

2,549件の閲覧回数
Pavel
NXP Employee
NXP Employee

Is there problem for console using on your board if Linux is loaded and started?


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,548件の閲覧回数
Pavel
NXP Employee
NXP Employee

It looks like that there is a problem of your terminal setting.

Check your terminal setting using the following pages:

http://www.armadeus.org/wiki/index.php?title=Connection_with_U-Boot_under_Windows

 

or

 

https://www.denx.de/wiki/DULG/SystemSetup

 

or

 

https://boundarydevices.com/just-getting-started/

 

 

Look at also attached file. Find the CONFIG_BOOTDELAY in this file. Perhaps the CONFIG_BOOTDELAY is set to 0 in your u-boot.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,548件の閲覧回数
matthuang
Contributor I

Hi Pavel,

I've checked and the terminal settings are correct. Also the CONFIG_BOOTDELAY value started from 10 so that's not the issue either.

I've taken a screenshot of the U-Boot message, perhaps that might be more telling of the issue that I have.

Thanks

Untitled.png

0 件の賞賛
返信