When I'm starting the LS1012ARDB board and the U-Boot message prompts me to hit any key to stop autoboot, I tried hitting keys but the terminal did not respond. I tried multiple cables so I don't think cable connection is the problem.
What might be causing this issue?
I looked at this thread but it didn't seem to help me:
https://community.nxp.com/thread/323089
Thanks
Is there problem for console using on your board if Linux is loaded and started?
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
It looks like that there is a problem of your terminal setting.
Check your terminal setting using the following pages:
http://www.armadeus.org/wiki/index.php?title=Connection_with_U-Boot_under_Windows
or
https://www.denx.de/wiki/DULG/SystemSetup
or
https://boundarydevices.com/just-getting-started/
Look at also attached file. Find the CONFIG_BOOTDELAY in this file. Perhaps the CONFIG_BOOTDELAY is set to 0 in your u-boot.
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Pavel,
I've checked and the terminal settings are correct. Also the CONFIG_BOOTDELAY value started from 10 so that's not the issue either.
I've taken a screenshot of the U-Boot message, perhaps that might be more telling of the issue that I have.
Thanks