Autoboot can not stop

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Autoboot can not stop

12,229 Views
wenlantang
Contributor III

When U-boot prints "Hit any key to stop autoboot:  10", enterring many key and many times, it still boots after 10 seconds. What might be the reason? Thank you.

Labels (1)
8 Replies

9,054 Views
hwrobel
NXP Employee
NXP Employee

The most common case for such issues IMHO is a bad USB<->UART converter on the host PC, assuming you are using one.

Most cheap ones are flaky and may or may not work reliably at rates higher than 9600.

A good indication if you have a cheap one or not is to see if keeps the COM port setting when removed from one USB port and plugged into another, and if it is designed by spec to handle rates up to ~1Mbps. If it enumerates again and sets up a different COM port, or if kbps is the fastest the spec says it can do, then you may want to look for a better one.

A setup with PuTTY and a good USB<->UART converter is absolutely reliable.

9,054 Views
wenlantang
Contributor III

And Windows Hyperterminal is used here with 115200-8-N-1.

By the way, you mentioned Putty, how to set the "flow control"? There is no "hardware" option for this, I tried "XON/XOFF", there is no response.

0 Kudos
Reply

9,051 Views
hwrobel
NXP Employee
NXP Employee

Regarding the driver, I had my Win 7 setup discover the correct FTDI driver, so I can’t comment on the FTDI drivers for download that you are referring to.

As for HyperTerminal, I never had a single positive experience with it, so I don’t use it. I have used TeraTerm in the past and currently use mostly Putty as it serves my needs well.

With regards to flow control, I left it as XON/XOFF in my settings, which is ok for my needs.

You never mentioned which board or setup you are using as target. You may want to check a different cable or the electrical signals on the target just to be sure that the host UART bits actually get to the target.

0 Kudos
Reply

9,051 Views
wenlantang
Contributor III

I use Win XP, that's different. The driver web http://www.ftdichip.com/Drivers/VCP.htm (FT2232) denotes XP should be supported.

Thank you and the target is TWR-P1025, I mentioned that in my reply to.

0 Kudos
Reply

9,051 Views
wenlantang
Contributor III

Thank you, the USB UART Virtual COM port is used, download from http://www.ftdichip.com/Drivers/VCP.htm (FT2232) as guided in FSL hardware getting started guide. Please advise?

0 Kudos
Reply

9,051 Views
shanmugamsundar
Contributor IV

Hi wenlan,

After booting can you able to access the console (i.e) typing some letters, if not check your Tx and Rx connection of your debug UART, there may be some loose conection or it may not be connected

Thanks,

shan

9,051 Views
wenlantang
Contributor III

No, cannot type in any letter. So there is connection issue in Tx of console? and no problem with Rx as there is log printed. How to fix? This is mini USB UART on TWR-P1025.

0 Kudos
Reply

9,051 Views
shanmugamsundar
Contributor IV

Hi wenlang,

For temporary solution to check whether it is working or not you can take a direct wire connection of debug uart's (Rx, Tx and Gnd) from any resistor point or any other possible points from the board and connect that to DB9 Female connector, from the DB9 Female  use USB to Serial converter, connect it to PC and check with minicom

Thanks,

shan

0 Kudos
Reply