1046 : FM_PORT_SetPCD: Failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1046 : FM_PORT_SetPCD: Failed

Jump to solution
1,321 Views
Chidananda22
Contributor IV

Hi All,

in my application I am doing port init.

It works in all LS1046 - 2088 and LX 2160.

In one our custom LS 1046 getting Below error.

the set_port_pcd(): FM_PORT_SetPCD: Failed,

        dpaa_fm_config(): Set Port PCD: Failed  

(gdb) bt

#0  0x0000000000974994 in FM_PCD_KgSchemeDelete (h_Scheme=0x0)

#1  0x00000000004aa754 in unset_pcd_netenv_scheme (dpaa_intf=dpaa_intf@entry=0x17ff73300)

#2  0x000000000097b0bc in dpaa_fm_config (dev=dev@entry=0x19063940 <rte_eth_devices>, req_dist_set=0)

#3  0x000000000097694c in dpaa_eth_dev_configure (dev=0x19063940 <rte_eth_devices>)

#4  0x00000000008c8d58 in rte_eth_dev_configure (port_id=port_id@entry=0, nb_rx_q=<optimized out>, nb_rx_q@entry=1,

    nb_tx_q=<optimized out>, nb_tx_q@entry=1, dev_conf=dev_conf@entry=0xffffeba9be48)

    

Thanks for help.

 

 

0 Kudos
Reply
1 Solution
1,270 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please configure FMC policy with the following commands.

fmc -x
fmc -c ./usdpaa_config_ls1046.xml -p ./usdpaa_policy_hash_ipv4_1queue.xml -a

Note: You need to modify usdpaa_config_ls1046.xml according to your custom board.

View solution in original post

1 Reply
1,271 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please configure FMC policy with the following commands.

fmc -x
fmc -c ./usdpaa_config_ls1046.xml -p ./usdpaa_policy_hash_ipv4_1queue.xml -a

Note: You need to modify usdpaa_config_ls1046.xml according to your custom board.