1046 : FM_PORT_SetPCD: Failed

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

1046 : FM_PORT_SetPCD: Failed

跳至解决方案
1,323 次查看
Chidananda22
Contributor IV

Hi All,

in my application I am doing port init.

It works in all LS1046 - 2088 and LX 2160.

In one our custom LS 1046 getting Below error.

the set_port_pcd(): FM_PORT_SetPCD: Failed,

        dpaa_fm_config(): Set Port PCD: Failed  

(gdb) bt

#0  0x0000000000974994 in FM_PCD_KgSchemeDelete (h_Scheme=0x0)

#1  0x00000000004aa754 in unset_pcd_netenv_scheme (dpaa_intf=dpaa_intf@entry=0x17ff73300)

#2  0x000000000097b0bc in dpaa_fm_config (dev=dev@entry=0x19063940 <rte_eth_devices>, req_dist_set=0)

#3  0x000000000097694c in dpaa_eth_dev_configure (dev=0x19063940 <rte_eth_devices>)

#4  0x00000000008c8d58 in rte_eth_dev_configure (port_id=port_id@entry=0, nb_rx_q=<optimized out>, nb_rx_q@entry=1,

    nb_tx_q=<optimized out>, nb_tx_q@entry=1, dev_conf=dev_conf@entry=0xffffeba9be48)

    

Thanks for help.

 

 

0 项奖励
回复
1 解答
1,272 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Please configure FMC policy with the following commands.

fmc -x
fmc -c ./usdpaa_config_ls1046.xml -p ./usdpaa_policy_hash_ipv4_1queue.xml -a

Note: You need to modify usdpaa_config_ls1046.xml according to your custom board.

在原帖中查看解决方案

1 回复
1,273 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Please configure FMC policy with the following commands.

fmc -x
fmc -c ./usdpaa_config_ls1046.xml -p ./usdpaa_policy_hash_ipv4_1queue.xml -a

Note: You need to modify usdpaa_config_ls1046.xml according to your custom board.