wdt reset

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

wdt reset

884 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Forrest on Tue May 22 11:31:37 MST 2012
Hi all,

mayby it is stupis question but,  is it reset generated by wdt same as hardware reset?

After HW reset all registers have default values defined in user manual.
Is it same if I reset mcu by wdt?

Thanks Forrest
0 项奖励
回复
2 回复数

873 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Forrest on Wed May 23 00:43:16 MST 2012
Thanks
0 项奖励
回复

873 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Tue May 22 11:54:01 MST 2012
User manual:


Quote:

When the Watchdog is in the reset mode and the counter underflows, the CPU will be reset, loading the stack pointer and program counter from the vector table [B][COLOR=Red]as in the case of external reset[/COLOR][/B].

0 项奖励
回复