wdt reset

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

wdt reset

886 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Forrest on Tue May 22 11:31:37 MST 2012
Hi all,

mayby it is stupis question but,  is it reset generated by wdt same as hardware reset?

After HW reset all registers have default values defined in user manual.
Is it same if I reset mcu by wdt?

Thanks Forrest
0 Kudos
Reply
2 Replies

875 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Forrest on Wed May 23 00:43:16 MST 2012
Thanks
0 Kudos
Reply

875 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Tue May 22 11:54:01 MST 2012
User manual:


Quote:

When the Watchdog is in the reset mode and the counter underflows, the CPU will be reset, loading the stack pointer and program counter from the vector table [B][COLOR=Red]as in the case of external reset[/COLOR][/B].

0 Kudos
Reply