wdt reset

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

wdt reset

890件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Forrest on Tue May 22 11:31:37 MST 2012
Hi all,

mayby it is stupis question but,  is it reset generated by wdt same as hardware reset?

After HW reset all registers have default values defined in user manual.
Is it same if I reset mcu by wdt?

Thanks Forrest
0 件の賞賛
返信
2 返答(返信)

879件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Forrest on Wed May 23 00:43:16 MST 2012
Thanks
0 件の賞賛
返信

879件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Tue May 22 11:54:01 MST 2012
User manual:


Quote:

When the Watchdog is in the reset mode and the counter underflows, the CPU will be reset, loading the stack pointer and program counter from the vector table [B][COLOR=Red]as in the case of external reset[/COLOR][/B].

0 件の賞賛
返信