use specific memory section memory to link a variable

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

use specific memory section memory to link a variable

3,791 次查看
Candice1
Contributor I

I'm having trouble in setting the section attribute of gcc to define that a variable should reside in a specific memory section instead of the default.

I'm using the arm cortex m3 LPC1759. I got the link files from LPCXpresso IDE, but I don't use it, I have my own makefile. The link files are:

Generic link file

INCLUDE "./link/LPCmem.ld" /* see below */

ENTRY(ResetISR)

SECTIONS
{
    /* MAIN TEXT SECTION */    
    .text : ALIGN(4)
    {
        FILL(0xff)
        __vectors_start__ = ABSOLUTE(.) ;
        KEEP(*(.isr_vector))
        
        /* Global Section Table */
        . = ALIGN(4) ;
        __section_table_start = .;
        __data_section_table = .;
        LONG(LOADADDR(.data));
        LONG(    ADDR(.data));
        LONG(  SIZEOF(.data));
        LONG(LOADADDR(.data_RAM2));
        LONG(    ADDR(.data_RAM2));
        LONG(  SIZEOF(.data_RAM2));
        __data_section_table_end = .;
        __bss_section_table = .;
        LONG(    ADDR(.bss));
        LONG(  SIZEOF(.bss));
        LONG(    ADDR(.bss_RAM2));
        LONG(  SIZEOF(.bss_RAM2));
        __bss_section_table_end = .;
        __section_table_end = . ;
        /* End of Global Section Table */
        

        *(.after_vectors*)
    } >FLASH
    
    .text : ALIGN(4)    
    {
         *(.text*)
        *(.rodata .rodata.* .constdata .constdata.*)
        . = ALIGN(4);
        
    } > FLASH

    /*
     * for exception handling/unwind - some Newlib functions (in common
     * with C++ and STDC++) use this. 
     */
    .ARM.extab : ALIGN(4)
    {
        *(.ARM.extab* .gnu.linkonce.armextab.*)
    } > FLASH
    __exidx_start = .;
    
    .ARM.exidx : ALIGN(4)
    {
        *(.ARM.exidx* .gnu.linkonce.armexidx.*)
    } > FLASH
    __exidx_end = .;
    
    _etext = .;
    
    /* DATA section for SRAM0 */
    .data_RAM2 : ALIGN(4)
    {
       FILL(0xff)
       *(.ramfunc.$RAM2)
       *(.ramfunc.$SRAM0)
        *(.data.$RAM2*)
        *(.data.$SRAM0*)
       . = ALIGN(4) ;
    } > SRAM0 AT>FLASH
    
    /* MAIN DATA SECTION */
    .uninit_RESERVED : ALIGN(4)
    {
        KEEP(*(.bss.$RESERVED*))
        . = ALIGN(4) ;
        _end_uninit_RESERVED = .;
    } > SRAM
    
    /* Main DATA section (SRAM) */
    .data : ALIGN(4)
    {
       FILL(0xff)
       _data = . ;
       *(vtable)
       *(.ramfunc*)
       *(.data*)
       . = ALIGN(4) ;
       _edata = . ;
    } > SRAM AT>FLASH

    /* BSS section for SRAM0 */
    .bss_RAM2 : ALIGN(4)
    {
        *(.bss.$RAM2*)
        *(.bss.$SRAM0*)
       . = ALIGN(4) ;
    } > SRAM0

    /* MAIN BSS SECTION */
    .bss : ALIGN(4)
    {
        _bss = .;
        *(.bss*)
        *(COMMON)
        . = ALIGN(4) ;
        _ebss = .;
        PROVIDE(end = .);
    } > SRAM
        
    /* NOINIT section for SRAM0 */
    .noinit_RAM2 (NOLOAD) : ALIGN(4)
    {
        *(.noinit.$RAM2*)
        *(.noinit.$SRAM0*)
       . = ALIGN(4) ;
    } > SRAM0 
    
    /* DEFAULT NOINIT SECTION */
    .noinit (NOLOAD): ALIGN(4)
    {
        _noinit = .;
        *(.noinit*) 
         . = ALIGN(4) ;
        _end_noinit = .;
    } > SRAM
        
    PROVIDE(_pvHeapStart = .);
    PROVIDE(_vStackTop = __top_SRAM - 0);
}

Memory definition file

/* Define each memory region */
MEMORY
{
  FLASH (rx) : ORIGIN = 0x0, LENGTH = 0x80000           /* 512K bytes */
  SRAM (rwx) : ORIGIN = 0x10000000, LENGTH = 0x8000     /* 32K bytes */
  SRAM0 (rwx) : ORIGIN = 0x2007c000, LENGTH = 0x8000    /* 32K bytes */
}

/* Define a symbol for the top of each memory region */
__top_FLASH = 0x0 + 0x80000;
__top_SRAM = 0x10000000 + 0x8000;
__top_SRAM0 = 0x2007c000 + 0x8000;

Above is the LPCmem.ld file included in the previous file.

I'm forcing the freertos heap variable to be in the custom section, like this:

static unsigned char ucHeap[ configTOTAL_HEAP_SIZE ]
        __attribute__((section(".data_RAM2")));

The linking of objects files are done without errors, but the variable isn't placed in the right memory position, how I could check with nm command:

...
10000028 d ucHeap
10002028 d uxCriticalNesting
...

I try to change the section to another that doesn't exist, just to check if the linker verifies the names, and apparently, it doesn't.

标签 (1)
0 项奖励
回复
1 回复

3,783 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Candice1 

Please check if this article can help you

https://community.nxp.com/t5/LPC-Microcontrollers-Knowledge/LPC-How-to-place-data-function-file-in-s...

Have a nice day

Jun Zhang

0 项奖励
回复