target not connected error.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

target not connected error.

791件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by [email protected] on Wed Jul 09 22:21:20 MST 2014
Hi ,
i am using LPC link2 debugger to connect to the Cortex m4 target and when i try to debug an application through lpcxpresso ide i get target not connected error.
My redlink probe says :

redlink>ProbeStatus
Index = 1
Manufacturer = NXP Semiconductors
Description = LPCLINK2 Redlink
VID = , PID=00
Path = \
IsOpen = TRUE
WireInitialized = TRUE
WireProtocol = SWD
CoresConfigured = TRUE
PacketSize = 64
Probe Reference Count = 0
HasSWV = FALSE
HasETM = FALSE
HasJTAG = TRUE
HasSWD = TRUE
Probe Type = REDLINK
redlink>exit
[Closed]

What are these two fields?
HasSWV = FALSE
HasETM = FALSE
what can be deducted from it?
0 件の賞賛
返信
1 返信

772件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Thu Jul 10 00:12:00 MST 2014
In the first place, make sure that the cable between your board and your probe is connected properly and the right way around.

Then see :

http://www.lpcware.com/content/faq/lpcxpresso/error-status-poll
http://www.lpcware.com/content/faq/lpcxpresso/regaining-debug-access

If you need further assistance, then please provide some details of your actual target, and also post the contents of your debug log and the actual error message in full:

http://www.lpcware.com/content/faq/lpcxpresso/debug-log

Regards,
LPCXpresso Support

0 件の賞賛
返信