target not connected error.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

target not connected error.

798 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by [email protected] on Wed Jul 09 22:21:20 MST 2014
Hi ,
i am using LPC link2 debugger to connect to the Cortex m4 target and when i try to debug an application through lpcxpresso ide i get target not connected error.
My redlink probe says :

redlink>ProbeStatus
Index = 1
Manufacturer = NXP Semiconductors
Description = LPCLINK2 Redlink
VID = , PID=00
Path = \
IsOpen = TRUE
WireInitialized = TRUE
WireProtocol = SWD
CoresConfigured = TRUE
PacketSize = 64
Probe Reference Count = 0
HasSWV = FALSE
HasETM = FALSE
HasJTAG = TRUE
HasSWD = TRUE
Probe Type = REDLINK
redlink>exit
[Closed]

What are these two fields?
HasSWV = FALSE
HasETM = FALSE
what can be deducted from it?
0 Kudos
Reply
1 Reply

779 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Thu Jul 10 00:12:00 MST 2014
In the first place, make sure that the cable between your board and your probe is connected properly and the right way around.

Then see :

http://www.lpcware.com/content/faq/lpcxpresso/error-status-poll
http://www.lpcware.com/content/faq/lpcxpresso/regaining-debug-access

If you need further assistance, then please provide some details of your actual target, and also post the contents of your debug log and the actual error message in full:

http://www.lpcware.com/content/faq/lpcxpresso/debug-log

Regards,
LPCXpresso Support

0 Kudos
Reply