stuck in the while(One_ms_tick>0) instruction

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

stuck in the while(One_ms_tick>0) instruction

542 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by PoolCop on Thu Jan 30 11:27:45 MST 2014
Hi guys,

I'm using timer0 IRQ handler to build delay.
I use a global static integer called "One_ms_tick" which is preset when entering the Delay_ms routine.
Then Delay_ms routine is waiting for "One_ms_tick" to be back to zero in a while statment.
Timer0 IRQ handler is in charge to decrease "One_ms_tick" every milli-seconds until zero.

As shown is the attached pict, even if "One_ms_tick" is decreased back to zero (I can see the value decreasing in debug mode), the Delay_ms routine stays stuck in the while instruction.

Any clue ?

Thanks
René

0 项奖励
回复
4 回复数

535 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by larryvc on Sat Feb 01 17:49:28 MST 2014

Quote: PoolCop
Adding some dumy statement such as writing something on the UART port makes the routine to work ????
Can not understand ....
Anyone has an idea ?


This probably due to the compiler making optimizations.  Like LabRat said Post your code.

Also are you sure that you have One_ms_tick as a global variable declared as
volatile int One_ms_tick;
?

Actually, to be more consistent with what you are using in the function Delay_ms(unsigned int count) I would declare it as
volatile unsigned int One_ms_tick;


either way One_ms_tick must be global and "volatile".
0 项奖励
回复

535 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LabRat on Sat Feb 01 11:58:20 MST 2014

Quote: PoolCop
Anyone has an idea ?



Just a crazy idea: post this astonishing project ???
0 项奖励
回复

535 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by PoolCop on Sat Feb 01 11:18:27 MST 2014
Thanks Capiman, but this has no effect...

Adding some dumy statement such as writing something on the UART port makes the routine to work ????
Can not understand ....
Anyone has an idea ?
0 项奖励
回复

535 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by capiman on Thu Jan 30 11:32:03 MST 2014
Have you used "volatile" for your global variable?
0 项奖励
回复