msc_rom example bug update

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

msc_rom example bug update

617件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ehughes on Tue Feb 08 18:42:25 MST 2011
I have been trying to get to the bottom of why the msc_rom example doesn't work with windows 7.   It was originally state on the forum hta tit might be because of the FAT 12 format.   I don't bleieve this is true as the "bootloader" seems to enumerate/wok just fine.

I have a 1343 xpresso board where I wired a M25PE16 device into the PIport.  I have gotten this device to read/write properly.  My goal is to get a 2MB flash drive with the built in ROM code.

My hardware has a 1k resistor on the D+ line to +3.3v as required.  I am also first starting the program and then connectin the USB cable (per instructions if one does not use the soft connect feature).

I notice that when I plug the device into a USB port,  the program will jump to the "HardFault"  irq handler continuously.   This is true under Wwindows XP and Windows 7.

Not sure what this means but I am going to look down that trail for awhile....
0 件の賞賛
返信
0 返答(返信)