lpc1769 demo code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

lpc1769 demo code

1,077 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by iantycoon on Sun Nov 06 18:52:33 MST 2011
may i know if anyone has the demo code which comes tgt with the lpc1769? the function it has are as follows:
[SIZE=3]
3 out of the 16 LEDs will always be lit and by tilting the board the LEDs that are lit will change (as a moving) bar. The way you move the board (in y-axis) will change the direction and speed of this bar.

The joystick can be used to draw on the OLED display. It is like moving a pen you never lift from the paper. By using the center key on the joystick the display is cleared.

Rotating the rotary switch will change which digit (0 to 9) is shown on the 7-segment display.

Pressing the SW3 button will start playing a melody.

Turning the trim potentiometer will turn on/off the RGB LEDs

I lost mine. appreciate if anyone can upload it. thanks
[/SIZE]
0 Kudos
Reply
1 Reply

711 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by atomicdog on Sun Nov 06 20:15:26 MST 2011
Did you check the NXP website?
0 Kudos
Reply