loading libraries in second Flash bank in LPC4357

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

loading libraries in second Flash bank in LPC4357

683 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by FutureDesign on Wed Jan 06 15:39:37 MST 2016
I have to load a pre compiled library of size 240kB in the second bank of the Flash. How can I do that?
By default the compiler/linker is placing in first flash bank.

Thanks 
0 Kudos
Reply
1 Reply

671 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Wed Jan 06 16:32:18 MST 2016

Here are the links to FAQs on lpcware.com which should help. The second link may not seem helpful, but you would use similar template commands to relocate objects/libraries to a different flash bank.

There are also a number of forum posts on this subject, there for the taking.

Freemarker Linker Script Templates

Relocating code from FLASH to RAM

Thanks and regards,
LPCXpresso Support
0 Kudos
Reply