LPC1769 USB device not recognized

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1769 USB device not recognized

1,083 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by yan6 on Thu Dec 26 14:47:33 MST 2013
Hi there, I'm having troubles getting the LPC-Link to connect via usb. I have tried it on Windows 7 & on XP, both with the same results. On both OS' I have tried manually to install the drivers by pointing the unknown device to the driver directory; I have tried installing the *.inf file and have tried to manually register the *.Dll's that are located in the driver directory, but receive an error. 

On the LPC board I am receiving 2 blinks on the LED while plugged into the computer

Can anyone offer some further suggestions
0 Kudos
Reply
0 Replies