is LPCXPRESSO free edition code limit?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

is LPCXPRESSO free edition code limit?

1,000件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lopezlop on Tue Feb 11 09:12:47 MST 2014
Hi guy's,

I am new to NXP (Hi NXP),
Can i compile and use my code in LPCXPRESSO 6.1.4 FREE edition OVER 256 kiloBytes?
of course i will use LPCXPRESSO included libraries (if there is),

i mean, i dont need to DEBUG my code

i just need to compile MY CODE and LPCXPRESSO libraries,  over 256K and generate a machine code (.Hex),then i will program by JLINK.
:)  :quest:
Best Regards.
0 件の賞賛
返信
2 返答(返信)

930件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lopezlop on Sat Mar 01 09:37:00 MST 2014
My experience on LPCXpresso 7:

unregistered version: build (and DEBUG) limited to 8k

FREE Version:
       DEBUG limited to 256k (user manual)
       Build Over 256k, (it seems unlimited), i build a 420k project.

Purchased license: of course go to LPCXpresso website for details.
0 件の賞賛
返信

930件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LabRat on Tue Feb 11 09:56:16 MST 2014
http://www.lpcware.com/lpcxpresso


Quote:
Free and Pro Editions

The popular Free Edition of LPCXpresso now offers many features previously only available in the premium Red Suite product (including C++ support), and doubles the [color=#f00]download limit to 256KB[/color].

0 件の賞賛
返信