JTAG with other LPC

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

JTAG with other LPC

738 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lgonzales52 on Wed Feb 10 11:32:15 MST 2010
I recently got a LPCXpresso board. I am also developing with an LPC2194 Quickstart board from Embedded Artists using Eclipse, gdb, and a wiggler paralel port jtag-interface. The cuestion is if I can use de USB JTAG of the LPCXpresso board with my old toolchain, or with other open source gdb based debugger ( insight for example)?.
Is there any document about the facts?
Thank you.
0 项奖励
回复
1 回复

724 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Thu Feb 11 00:49:44 MST 2010
The LPCXpresso IDE supports only a small subset of the LPC2xxx family, and the LPC2194 is not amongst them.

The LPC-Link interface is currently only supported in LPCXpresso (and Red Suite).

There is an upgrade product from Code Red (Red Suite 3 - currently in beta) that supports the LPC2xxx family and LPC-Link.
0 项奖励
回复