how to program DALI Master

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to program DALI Master

2,220件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jx1 on Mon May 27 03:00:06 MST 2013
Hi everyone,

anyone knows how to program the DALI Master board(LPC1343) by using the LPCXpresso board? :confused:
0 件の賞賛
返信
8 返答(返信)

2,078件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LabRat on Mon Dec 30 10:18:46 MST 2013

Quote: sassi
Can you explain to me what was your solution.




Quote:
target which is still connected to the LPC link



Sounds like he didn't separate LPC-link from target board before trying to use it for another target...

See: http://www.lpcware.com/content/forum/recommendation-of-how-to-split-up-the-board
0 件の賞賛
返信

2,078件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by sassi on Mon Dec 30 10:00:59 MST 2013
Hello, i have the same problem as you, I am using lpclink which is linked to lpcxpresso board and i want to program the dali master. Can you explain to me what was your solution.
0 件の賞賛
返信

2,078件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jx1 on Tue May 28 18:55:11 MST 2013
I think the problem is my LPCXpresso target which is still connected to the LPC link therefore it could not connect to an external JTAG interface. Thanks everyone for providing solutions.
0 件の賞賛
返信

2,078件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by frame on Tue May 28 06:19:13 MST 2013
Is the wiring of the debug adapter to the target correct  - and have you double-checked this ?

Is the target powered ?

Decide where to power your target from.
For me, it worked powering the target ([B]exactly this[/B] Dali master board) from USB,
and disabling the debug adapter as supply (lpclink2 in my case).
0 件の賞賛
返信

2,078件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Tue May 28 00:24:59 MST 2013

Quote:
02: Failed on connect: Ee(07). Bad ACK returned from status - wire error.
Emu(0): Connected. Was: None. DpID:     EDB6. Info: HID64HS12

Ever though of using search? There are many instances of this question being asked and answered on the forum.
0 件の賞賛
返信

2,078件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by serge on Mon May 27 23:31:09 MST 2013

Quote:
I tried to debug so as to program the DALI master board but it shows me this error. What does it mean?:(

02: Failed on connect: Ee(07). Bad ACK returned from status -[COLOR=red] wire error[/COLOR].
Emu(0): Connected. Was: None. DpID: EDB6. Info: HID64HS12



What is wrong with 'wire error'? :rolleyes:
0 件の賞賛
返信

2,078件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jx1 on Mon May 27 23:07:27 MST 2013
I tried to debug so as to program the DALI master board but it shows me this error. What does it mean?:(

02: Failed on connect: Ee(07). Bad ACK returned from status - wire error.
Emu(0): Connected. Was: None. DpID:     EDB6. Info: HID64HS12
0 件の賞賛
返信

2,078件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by frame on Mon May 27 04:38:33 MST 2013
By making an adapter from the 1x8 output of the LPC-Link to the 2x5 socket connector.
Some soldering might be required.
0 件の賞賛
返信