float representation compatible with IEEE ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

float representation compatible with IEEE ?

820 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by devidasbhonde on Tue Jan 08 09:27:00 MST 2013
Hi, I wish to know whether float representation of a single precision number is compatible with IEEE standard ?
I require to connect an AVR card to LPC1343 daughter board & includes exchange of FP numbers. If the binary representation of both are same then only it would be possible. (The AVR is programmed in BASCOM, which follows IEEE).
Thanks,
Devidas
0 项奖励
回复
2 回复数

814 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by devidasbhonde on Tue Jan 08 09:59:53 MST 2013
Thank you.
It is reassuring to hear this before actually connecting the hardware.
Regards,
Devidas
0 项奖励
回复

814 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Tue Jan 08 09:53:37 MST 2013
yes, they are IEE754
0 项奖励
回复