float representation compatible with IEEE ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

float representation compatible with IEEE ?

821 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by devidasbhonde on Tue Jan 08 09:27:00 MST 2013
Hi, I wish to know whether float representation of a single precision number is compatible with IEEE standard ?
I require to connect an AVR card to LPC1343 daughter board & includes exchange of FP numbers. If the binary representation of both are same then only it would be possible. (The AVR is programmed in BASCOM, which follows IEEE).
Thanks,
Devidas
0 Kudos
Reply
2 Replies

815 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by devidasbhonde on Tue Jan 08 09:59:53 MST 2013
Thank you.
It is reassuring to hear this before actually connecting the hardware.
Regards,
Devidas
0 Kudos
Reply

815 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Tue Jan 08 09:53:37 MST 2013
yes, they are IEE754
0 Kudos
Reply