Workspace naming

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Workspace naming

1,125件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by capstone on Thu Jun 12 11:49:37 MST 2014
Win 7-64/LPCXpresso v7.2.0

Workspace considerations

Is there a way to locate or visually see the current Workspace name?

- when more than one IDE launched, the Switch Workspace provides a list of previous selections, but may not have this
current selection as the first item.

Since the Workspace is a Logical assignment, how can the current Physical location be discovered?

How can the Name assigned to the Workspace be changed?

Thanks
0 件の賞賛
返信
2 返答(返信)

1,115件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by capstone on Thu Jun 12 16:59:18 MST 2014
Thanks! This was so simple; now the Workspace name is available.  ;-)
0 件の賞賛
返信

1,115件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Thu Jun 12 13:52:55 MST 2014
The information in this article equally applies to LPCXpresso:

http://mcuoneclipse.com/2012/08/01/show-workspace-location-in-the-title-bar/

You just need to replace references to eclipse.ini with lpcxpresso.ini.

Regards,
LPCXpresso Support

0 件の賞賛
返信