Workspace naming

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Workspace naming

1,123 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by capstone on Thu Jun 12 11:49:37 MST 2014
Win 7-64/LPCXpresso v7.2.0

Workspace considerations

Is there a way to locate or visually see the current Workspace name?

- when more than one IDE launched, the Switch Workspace provides a list of previous selections, but may not have this
current selection as the first item.

Since the Workspace is a Logical assignment, how can the current Physical location be discovered?

How can the Name assigned to the Workspace be changed?

Thanks
0 Kudos
Reply
2 Replies

1,113 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by capstone on Thu Jun 12 16:59:18 MST 2014
Thanks! This was so simple; now the Workspace name is available.  ;-)
0 Kudos
Reply

1,113 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Thu Jun 12 13:52:55 MST 2014
The information in this article equally applies to LPCXpresso:

http://mcuoneclipse.com/2012/08/01/show-workspace-location-in-the-title-bar/

You just need to replace references to eclipse.ini with lpcxpresso.ini.

Regards,
LPCXpresso Support

0 Kudos
Reply