Using LPC-Link Standalone

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using LPC-Link Standalone

716 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ian Stroud on Fri Feb 18 03:15:14 MST 2011
I need to distribute executable files to colleagues who are also using the LPCXPRESSO development boards with with the embedded LPC-LINK JTAG adapter.

Is there a standalone utility that can be used to download executable files or can LPC-LINK only be used from the LPCXPRESSO IDE?
0 Kudos
Reply
1 Reply

700 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Fri Feb 18 05:36:55 MST 2011

Quote:
...who are also using the LPCXPRESSO...



Did you try 'Program Flash' within IDE (little chip icon) and *.axf file ?

or

'Using the command line flash programming tool':

http://support.code-red-tech.com/CodeRedWiki/CommandLineFlashProgramming
0 Kudos
Reply