Using LPC-Link Standalone

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using LPC-Link Standalone

704件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ian Stroud on Fri Feb 18 03:15:14 MST 2011
I need to distribute executable files to colleagues who are also using the LPCXPRESSO development boards with with the embedded LPC-LINK JTAG adapter.

Is there a standalone utility that can be used to download executable files or can LPC-LINK only be used from the LPCXPRESSO IDE?
0 件の賞賛
返信
1 返信

688件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Fri Feb 18 05:36:55 MST 2011

Quote:
...who are also using the LPCXPRESSO...



Did you try 'Program Flash' within IDE (little chip icon) and *.axf file ?

or

'Using the command line flash programming tool':

http://support.code-red-tech.com/CodeRedWiki/CommandLineFlashProgramming
0 件の賞賛
返信