Use a $8 dongle to program LPCXpresso under Linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Use a $8 dongle to program LPCXpresso under Linux

1,710 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Bingo600 on Thu Apr 14 11:45:25 MST 2011
Hi Guyzz

Just started using my LPCXpresso under linux , full debugging & programming via Versaloon (SWD) and a $8 STM8S-Discovery board (Has a 72Mhz arm on it).
The STM8S-Discovery , like the LPCXpresso has an onboard debugger (A 72Mhz ARM)  that connects direct via USB.

The ARM part of the board is converted to a Versaloon SWD dongle.

I'm using Codesourcery-Lite , NXP CMSIS v2.0 and OpenOCD (where Versaloon has SWD support)

http://www.avrfreaks.net/index.php?name=PNphpBB2&file=viewtopic&p=817534#817534

The STM32VL-Discovery can be converted as well.

http://www.versaloon.com/bbs/viewtopic.php?f=2&t=17

The Xpresso is a nice board , but i still don't get the part about making the debugger closed.

The 1768 only needs 2 SWD wires (SWDIO & SWCLK) , but i think the Cortex-M0 needs reset also , this one is easiest to get (solder on) with the STM32VL-Discovery.

This is also working on a MAC.


/Bingo
0 Kudos
Reply
6 Replies

1,640 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Tue Apr 26 05:36:31 MST 2011
German Embedded Artists Distributor:

http://www.watterott.com/

isn't selling things like LPCXpresso1227, but 'crap' from the largest European semiconductors supplier:

http://www.watterott.com/de/STM8S-Discovery
0 Kudos
Reply

1,640 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by electronica@tdnet on Mon Apr 25 04:14:20 MST 2011

Quote: NXP_Europe
Guys, please this is a NXP website and we surely don't appreciate it when you're promoting ST stuff (crap ;)).

So please take this discussion elsewhere!!

Kind regards,



You are right, but how to get it running under Linux,
if the CodeRed stuff works only under i386 and not ARM?
0 Kudos
Reply

1,640 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Europe on Mon Apr 25 02:21:21 MST 2011
Guys, please this is a NXP website and we surely don't appreciate it when you're promoting ST stuff (crap ;)).

So please take this discussion elsewhere!!

Kind regards,
0 Kudos
Reply

1,640 Views
lpcware
NXP Employee
NXP Employee
0 Kudos
Reply

1,640 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by electronica@tdnet on Sun Apr 24 17:16:43 MST 2011

Quote: Bingo600
Hi Guyzz
Just started using my LPCXpresso under linux , full debugging & programming via Versaloon (SWD) and a $8 STM8S-Discovery board (Has a 72Mhz arm on it).
/Bingo



Where do you have gotten the dongle for this price?

I was on the Versaloon Website and there is only the "Versaloon Mini"
available and it cost 30 US$ + 20 US$ shiping

Note: I am in France and if someone can send it to me much less expensive
      as on this website please feel free to contact me.

Greetings
Michelle
0 Kudos
Reply

1,640 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Luis Digital on Thu Apr 14 12:45:43 MST 2011

Quote: Bingo600
Hi Guyzz

Just started using my LPCXpresso under linux , full debugging & programming via Versaloon (SWD) and a $8 STM8S-Discovery board (Has a 72Mhz arm on it).
The STM8S-Discovery , like the LPCXpresso has an onboard debugger (A 72Mhz ARM)  that connects direct via USB.

The ARM part of the board is converted to a Versaloon SWD dongle.

I'm using Codesourcery-Lite , NXP CMSIS v2.0 and OpenOCD (where Versaloon has SWD support)

http://www.avrfreaks.net/index.php?name=PNphpBB2&file=viewtopic&p=817534#817534

The STM32VL-Discovery can be converted as well.

http://www.versaloon.com/bbs/viewtopic.php?f=2&t=17

The Xpresso is a nice board , but i still don't get the part about making the debugger closed.

The 1768 only needs 2 SWD wires (SWDIO & SWCLK) , but i think the Cortex-M0 needs reset also , this one is easiest to get (solder on) with the STM32VL-Discovery.

This is also working on a MAC.


/Bingo



Thanks for the information.

I had already read something like that out there. You can program the Cortex-M0 without reset, but it's a hassle to do it manually.
0 Kudos
Reply