USB secondary bootloader & Android OS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB secondary bootloader & Android OS

1,035件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Franky on Wed Mar 13 13:31:02 MST 2013
Hello Guys, I need some support around firmware transfer to uC with Android OS. I have problem with firmware transfer (*.bin) from Android tablet to uC NXP LPC1768. The point is that the android PC find the uC memory and I can transfer the firmware. But after reset the uC wont execute user firmware. The firmware loads into the uC successfully.
The whole firmware transfer process works on windows PC without any problems.
Are there any compatibility problems, or settings to overcome this problem on Android tablet?
I think I'm not only one who was tried to transfer *.bin file to uC from Android tablet.
0 件の賞賛
返信
2 返答(返信)

988件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Franky on Thu Mar 14 23:51:37 MST 2013
Thank you Tsuneo.
0 件の賞賛
返信

988件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Tsuneo on Thu Mar 14 11:10:44 MST 2013
The FAT file system support on Android derives from Linux code.
And then, the workaround for Linux will be applied.

http://www.nxp.com/documents/application_note/AN10986.pdf
[I]The most general workaround is to overwrite the firmware.bin in place.[/I]

Tsuneo
0 件の賞賛
返信