USB communications

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB communications

681件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Andrew24 on Sat Mar 27 11:07:40 MST 2010
Hallo. I 'm developing a project on LPC1343 to acquire some data from a sensor, and then send the value through the USB to computer. What is the simplest way to do this? can i use the same usb cable for communications that i use to program and debug? or do i need to use the pins USB_DM, USB_DP?
0 件の賞賛
返信
1 返信

638件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Sat Mar 27 13:46:35 MST 2010
The LPCXpresso's debug USB connection is dedicated to debug, you cannot use it for your own purposes.

You need to connect to the USB pins on the LPC1343 chip itself, by either adding you own hardware, or connecting to an Embedded Artists LPCXpresso baseboard.

I would suggest a good starting place for more information would be the two LPC1343 apps notes available from NXP's website:

http://ics.nxp.com/support/documents/microcontrollers/

or more directly at:

http://ics.nxp.com/support/documents/microcontrollers/zip/an10905.zip
http://ics.nxp.com/support/documents/microcontrollers/zip/an10904.zip

Regards,

CodeRedSupport
0 件の賞賛
返信