USB vendor id question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB vendor id question

1,092 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by SolomonViveros on Wed Feb 16 11:39:58 MST 2011
The concept of designing out the FTDI FT232 with the LPC134x is a neat one but then topic of vendor id arises; if I were to have a design that included usb is it first necessary to obtain a VID or are there generic numbers I can use?
0 Kudos
Reply
3 Replies

1,068 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Luis Digital on Mon Feb 21 06:02:26 MST 2011
1,2,3

I posted a comment a few days ago here, but do not see it.

Please administrator, put the message.
0 Kudos
Reply

1,068 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Luis Digital on Sat Feb 19 13:58:26 MST 2011
Hello,

There are resellers that offer low prices, but the ID remains of his company. Another option is to recycle the IDs of other devices that perform the same function, such as your mause, if your application is a mouse.

Something similar is done with MAC addresses.

<a href="http://www.mcselec.com/index.php?page=shop.product_details&flypage=shop.flypage&product_id=92&option...">USB id reseller</a> I think I have seen others, but I can not remember.

NXP should provide in their chips a generic ID.
0 Kudos
Reply

1,068 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ljose on Sat Feb 19 12:28:23 MST 2011
During development you can generate any random USB vendor ID. Keep a higher value to reduce chance of conflicting with any existing IDs

But when you make a commercial product you will have to procure one - http://www.usb.org/developers/vendor/
0 Kudos
Reply