USB Connection Lost after Debug with Linux

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB Connection Lost after Debug with Linux

760件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by garfunx on Wed May 29 02:50:15 MST 2013
Hi,

I have the following behaviour using Linux LPCXpresso 5.1.2.

- Start Debug
- Stop Debug
- Fail to flash the component:

02: Failed on connect: Ee(07). Bad ACK returned from status - wire error.
Emu(0): Conn&Reset. Was: None. DpID:    30003. Info: LPCLINK_1_1

I have to unplug LPCXpresso board and plug it back.

I don't know if this forum is the best place to report this kind of problems. Please let me know if there is a better way to report this problem.
0 件の賞賛
返信
1 返信

752件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Wed May 29 03:07:03 MST 2013
This probably mean that you application is using one of the debug (SWD) pins for another purpose, or you have got the device into a bad state. Look at
http://support.code-red-tech.com/CodeRedWiki/DebugAccessChip
0 件の賞賛
返信