UART for ISP

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

UART for ISP

3,589 次查看
prachipanse
Contributor III

Hi,

I need to program the on-chip flash of LPC1313FBD48/01 device. I have connected the SWCLK and the SWDIO pins to the debug connector. The UART interface is connected to some other peripheral. I have some queries regarding the same:

Is it necessary to use ISP or IAP modes to program the flash or can it be done without that?

Also, if ISP mode is to be used, how is the UART interface to be used for this purpose?

Thanks and Regards,

Prachi

标记 (3)
0 项奖励
回复
2 回复数

2,441 次查看
lpcxpresso_supp
NXP Employee
NXP Employee

If you have connected up the SWD signals, then you could debug using LPCXpresso IDE (or MCUXpresso IDE) plus a debug probe - such as LPC-Link2 : LPC-Link2|NXP 

To make sure you have implement appropriate debug/reset circuitry, you might also want to check out the FAQ : Design Considerations for Debug 

If you want to program using ISP, then you will probably want to look at a utility such as FlashMagic : Flash Magic - Welcome (external site).

Regards,

LPCXpresso Support

0 项奖励
回复

2,441 次查看
prachipanse
Contributor III

Thanks. This clarifies my query.

0 项奖励
回复