Suspend button becomes grayed out during debug

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Suspend button becomes grayed out during debug

781件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ECamino on Tue Jul 16 06:16:00 MST 2013
Hi,

When debugging, one of my interrupts causes the suspend button to gray out. I can see the application is still running and is not trapped in a hard fault or anything. Without yellow suspend, I can't stop the program to debug.  I have to hit terminate.  Why is it happening and what do I do to fix it?

Version: LPCXpresso v4.2.3 [Build 292] [30/05/2012]

Thanks,

EC
0 件の賞賛
返信
1 返信

758件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Tue Jul 16 08:01:07 MST 2013
The button will become grayed if you have not got the "application.axf" entry selected in the Debug View.

BTW: v4.2.3 is very out of date. Latest version is v5.2.6
0 件の賞賛
返信