Slow import and build of projects

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Slow import and build of projects

787 Views
yunusishak
Contributor I

Hello,

I am using LPC 6.1.4_194 version of LPC Expresso for an assignment. I am experiencing incredibly long times for importing projects. The loading bar load up to almot 100% then it'll freeze for some time before it completes.

Once I have imported my project the build time takes a very long time as compared to the laptop of my partner. I have a much newer PC that is less than 1 year old. His is almost 5 years.

Labels (1)
0 Kudos
Reply
1 Reply

700 Views
lpcxpresso_supp
NXP Employee
NXP Employee

The normal cause of such issues is an issue with virus checkers. If you use the "Search Widget" within this forum space, and look for something like "slow build", this will bring up some previous reports of such issues which would probably be worth you browsing - for example: https://community.nxp.com/message/770106 

Note that you are using a very old version of the IDE - the current is LPCXpresso IDE v8.2.2.

Regards,

LPCXpresso Support

0 Kudos
Reply