Slow import and build of projects

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Slow import and build of projects

775件の閲覧回数
yunusishak
Contributor I

Hello,

I am using LPC 6.1.4_194 version of LPC Expresso for an assignment. I am experiencing incredibly long times for importing projects. The loading bar load up to almot 100% then it'll freeze for some time before it completes.

Once I have imported my project the build time takes a very long time as compared to the laptop of my partner. I have a much newer PC that is less than 1 year old. His is almost 5 years.

ラベル(1)
0 件の賞賛
返信
1 返信

688件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

The normal cause of such issues is an issue with virus checkers. If you use the "Search Widget" within this forum space, and look for something like "slow build", this will bring up some previous reports of such issues which would probably be worth you browsing - for example: https://community.nxp.com/message/770106 

Note that you are using a very old version of the IDE - the current is LPCXpresso IDE v8.2.2.

Regards,

LPCXpresso Support

0 件の賞賛
返信